This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教BQ24103充电电流太小的问题!为什么这么久都没有大神回复???



根据附件电路,插入电压为7V左右的锂电池,PG灯和充电灯正常亮起,Rsense电阻两端电压只有40mV,根据datasheet说明,理论上应该是130mV左右。

其他关键信号电压如下:Iset1电阻两端电压1V,Iset2电阻两端电压0.46V,温度检测端电压1.5V(电池内470欧热敏电阻),TTC端电压0.67V,电源输入电压9.2V.

 

另:1、这个电路在另外一块电路板上能正常充电(原理图基本一样,同一批芯片),这个电路焊了两块电路板都是这样。

        2、Iset2电阻两端电压手册不是说是0.1V么?但是我在 1 中描述的能用的电路上面,测量是1V左右,跟Iset1电阻两端电压基本一样,请解释。

        3、附件的PCB图不是最终版本,最终版本加宽了电源输入路径的走线(40mil)。

       谢谢!!!!!!

power.pdf