This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27541的MATHCAD怎么用?

Other Parts Discussed in Thread: BQ28400

BQ27541的MATHCAD怎么用?我以为是一个软件呢,下载的的全是EXCEL表格,按照说明打开 chemselect_cont.mcd却打不开,有没有更详细的说明,或图文指导啊,另外请推荐一款外形较小,通讯协议为I2C 用于2节锂电池电量管理的IC。

  • MATHCAD是一个第三方软件,MATHCAD15和MATHCAD14都可以支持计算chem-id,你可以认为 chemselect_cont.mcd是基于MATHCAD的一个程序,安装MATHCAD软件后点击就可以打开这个文件,ctrl+F9建就能执行计算出结果(运算时间可能需要数分钟)。实际操作中,你只需要将自己log的数据里的时间电压电流温度替换到里面的chemselect_cont_Arbin_exaple.xls对应的列里(注意单位转换),再按ctrl+F9就可以看到结果。如果没有这个软件请将符合CHEM-ID要求的log文件贴上我帮你计算一下(充满-静置-C/5或者C/10放电-静置5小时)。2节如果需要带保护功能的话一般体积都比较大,可以考虑BQ28400,这个是CEDV算法的,参数配置比较简单。如果单纯计量也有采用bq27541+运放分压的方案(要求不高甚至可以考虑只计量其中一节的电量)。