我们在设计外围电路的时候也用到了UCD9248PFC(官网上看到UCD9240PFC停产了),然后在论坛上看到一个帖子说UCD92xx系列的芯片(电源控制器)
,内部有firmware(程序),还需要通过Fusion软件配置相关信息(配置信息出厂是空的)才能正常输出电压
那么是否意味着只有裸芯片那么UCD92xx系列芯片无法正常输出电压?如果想输出正常电压一定要配合Fusion软件才能正常工作?
如果不使用Fusion软件时候就不能够使用UCD9248PFC芯片输出正确的电压?
盼解惑,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们在设计外围电路的时候也用到了UCD9248PFC(官网上看到UCD9240PFC停产了),然后在论坛上看到一个帖子说UCD92xx系列的芯片(电源控制器)
,内部有firmware(程序),还需要通过Fusion软件配置相关信息(配置信息出厂是空的)才能正常输出电压
那么是否意味着只有裸芯片那么UCD92xx系列芯片无法正常输出电压?如果想输出正常电压一定要配合Fusion软件才能正常工作?
如果不使用Fusion软件时候就不能够使用UCD9248PFC芯片输出正确的电压?
盼解惑,谢谢
您好,问下扫描的时候显示以下错误:提示选择到的地址为126,查了以下地址126是不推荐使用的地址,然后硬件设计的地址不是126,
错误提示如下:
address 126, the sync functions have been disabled
If you configured your address selection reistor for this address and behavior intentionally, please ignore this warning.
If you did not configure address 126 through resistors then the device has selected this address because it is the "fallback" address assigned when an invalid address selection resistor is detected
谢谢Neli的回答,
我有两个一样的ucd92xx连接在一个pmbus接口上,然后能扫描到其中一个,我已经烧了一个样例程序进去了(怕出错),然后需要在这两个里面分别烧录配置程序,
现在我运行后显示扫描到2个器件,然后点击进来出现烧录的的样例程序,但现在要烧录配置程序,是直接点击file-import,然后会让你选择烧录文件类型,选择需要烧录的文件,然后是烧录
没有看到这种器件选择的情况
您是在什么时候出现上面界面的?我试了好多次都没有发现器件选择
ps:我是Fusion Design online/offline v1.8 版本的
谢谢