This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

相移全桥谐振电感的设计问题



您好:参考TI相移全桥实现条件的介绍,设计一款相移全桥拓扑DCDC电路,输入输出为:DC输入400V,输出30V-110V/20A可调,谐振电感LR的计算过程如下:选用的4 IGBT模块作为H桥开关,该开关器件参数Coss=0.125nF,假设设定输出最小电流为2A时仍连续工作,变压器寄生电容不计的情况,CR=8/3*0.12nF=0.33nF,变压器变比设为11:2,Iprimin=2/11*2A=0.364A,Vinmax=400V*(1+12.5%)=450V计算,按照LRprimin2>8/3Coss*Vinmax 2条件计算,则得到的LR>0.33nF*450*450/(0.364*0.364)=504mH,这样算出来的谐振电感是不是太大了,算法中哪里不对,麻烦专家给指点一下,万分感谢!