BQ25570资料中的SLUC484可以帮助我们选择电阻,这个SLUC484是什么资料,都找不到呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SLUC484是产品线提供的一个excel工具,方便配置bq25570各种参数,参考此链接http://www.ti.com/lit/zip/sluc484
图6中的D,S应该是写反了,影响不大,主要说明是P管。
VOUT-EN控制的是BUCK CONVERTER,如果不使能,VOUT没有输出,IBUCK也没有输出,上管应该关闭的。BOOST电路仍可以工作,VSTOR有输出。
1.VOUT和LBUCK在内部并不是连在一起的,LBUCK是连接降压的输出控制MOS管的源极(或是漏极),VOUT接输出控制MOS管的栅极,VOUT更像一个反馈,不知道我这样理解对不对,因为看图上VSTOR上的电压不会到vout上的
2.当VOUT-EN不使能时,VSTOR上的电压会是多少,这时只与前面的升压电路有关系,而与VOUT-SET外面的两个电阻没有关系了是吧?
3.资料中的turn on 对于VSTOR和VBAT之间的MOS管事导通还是断开?当该MOS管导通时,源极和漏极就没有压差了,就相当于一条导线?