前段时间使用了TPS7A4901,输入端加+28V电,输入端分两路供电,1路给TPS7A4901,电流大约30mA,另一路给加热块,加热块的电流大约1.2A,在使用时发现如果电源断电后重新加电,则4901很容易烧毁,不知道是什么原理,如果在电源的输入端与TPS7A4901的输入端之间串联一个电阻是否可以改善?谢谢.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
前段时间使用了TPS7A4901,输入端加+28V电,输入端分两路供电,1路给TPS7A4901,电流大约30mA,另一路给加热块,加热块的电流大约1.2A,在使用时发现如果电源断电后重新加电,则4901很容易烧毁,不知道是什么原理,如果在电源的输入端与TPS7A4901的输入端之间串联一个电阻是否可以改善?谢谢.
你这个问题很可能是由于电热块重新上电时,瞬间启动电流较大(电热丝冷电阻较小,上电启动电流会远大于1.2A),浪涌电流打坏了LDO,这种情况LDO前面串接一个电阻可以改善一些。也有可能上下电时你的+28V电源波动较大,有电源尖峰打坏了LDO,建议再加个TVS管试试。
你可以试试加热块上电后再给LDO上电是否会出现烧毁的情况。