Other Parts Discussed in Thread: BQ24296, BQ24196
你好,刚开始接触手持式仪器,所以不太了解充电芯片和电量检测芯片,希望推荐几个充电芯片和电量检测芯片。
我用的是2节18650并联锂电池,电压3.7V,每节容量3000mAh,希望用USB电压和适配器充电,要求主机控制。
还有就是要求现有开发资料比较多或者比较主流的芯片。
3Q
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
充电电流需要多少,适配器输入电压最高是多少?如果没有具体规格可以看下bq24296是否能满足需求。
电量检测芯片目前使用比较多的有bq27541,但是bq27541需要比较多的开发经验。如果楼主第一次接触这一方面,建议可以选择比较简单的电量计,比如bq27441.谢谢!
谢谢,打算用的适配器电压在5V-12V之间,输出电流在1A-3A之间
12V的适配器需要使用bq2419X系列,例如bq24196
请问bq27541和bq27441之间有什么区别吗?除了高位电流检测外?