This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z110问题6



  • TI技术支持:

收到您2014-2-13的回复,现将祥细情况说一下:

1)    我将CC THRESHOLD设为超威蓄电池型号为6-DZM-20的标准容量0X4E20(20000MAH),在学习过程中第一次放电到终点电压时CYCLE COUNT计数器的值为0.库仑计数值总是在16383MAH.无论放电电流多大,库仑计数器总是一样的还为16383MAH.当库仑计数器记满到16383MAH后,SOC,FCC,RM都保持不变.直到终止电压后,SOC和RM才变为0.这是为什么?请TI公司技术人员帮助分析一下.

2)    QMAX CELL 0  应该设定为多大?铅酸蓄电池超威电池的标称容量为0X4E20(20000MAH).无论起始QMAX CELL 0 设定为多大的值,学习时第一次放电后QMAX CELL 0 的值均变为17000MAH左右.对吗?能举个例说明吗?

谢谢!

  • 做实验前先把QMAX CELL0和CELL1设定为20000mAH,全程记录充放电数据,可以每10秒记录一次电压,电流,温度,RM,FCC和SOC的数据,QMAX CELL0的更新值是和实际放电电量相关的,建议你所有的数据贴上来看看。