This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LT1945输入为3V至6.5V,输出正负12V,输出电流有多大?



我考虑用LT1945设计产品的电源,前端输入用4节电池供电。输出用LT1945产生正、负12V电源,-12V需要10mA,+12V需要不超过100mA。

看LT1945手册的指标,其中Switch VCESAT  ISW = 300mA,Switch Current Limit为350mA。

请问:1、是不是表明最大输出电流有300mA?这个Switch 表示的是哪部分的电流?

2、我上述方案,LT1945是否可以满足?

3、如果不可以满足,那我上述方案输出电流最大有多少mA?

4、如果我上述方案可以满足要求,为什么手册中的典型电路的输出电流只标注了10mA和20mA呢?

谢谢。