This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

寻找输入输出是12V的“移动电源”管理芯片

Other Parts Discussed in Thread: BQ24195

BQ24195是一款比较优秀的移动电源管理芯片,输入5V输出5V的供电方式,并且支持OTG供电方式。

请问TI工程师,有没有输入12V,输出12V(2A),电池是单节或者两串的电源管理芯片,功能和BQ24195类似。

即:**适配器12V输入,给电池充电,并且可以直接供给输出。

       **拔下适配器时,电池通过升压,输出12V。 谢谢~~~

  • 你好,这个规格需求目前没有集成的方案,只能用独立器件去搭建。

    用一个带有功率路径管理的充电器 来给电池充电, 然后电池的输出端加一个12V的boost电路。谢谢!