今天一直在看BQ24190的数据手册,还是有一些问题没看明白,向各位前辈请教。
1、boost mode 和buck mode。数据手册23页最后一段话,运行boost mode 时,VBUS变成输出5V了,我不太理解,那SYS电压和电流是没有了还是什么?
2、D+、D-在检测电源的时候会不会影响USB通信。
3、USB供电充电电流是不是不能达到4.5A的,输入电流和充电电流是什么关系。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.Vsys电压还是和正常一样,只是从电池boost升压一个5V到VBUS给外部供电,正常的charger工作时一个buck电路,反过来看就是一个boost的电路
2.有可能,如果系统需要USB通信,可以选择bq24192这种PSEL控制的charger,由主机判断出USB类型(是数据USB口还是adapter口)然后决定充电电流大小
3.4.5A应该是指电池充电电流,但是注意要达到这个电流需要比较好的layout散热,并且adapter应该是高压的(9V/12V),5V的adapter话这个电流太大了,如果不考虑系统端耗电,可以认为输入电流*输入电压*效率=充电电流*电池电压