Other Parts Discussed in Thread: TPS75003
你好,我打算使用TI的TPS75003芯片为altera的EP3C10芯片供电。电路采用了芯片手册FIG2所示的典型电路。在空载情况下测试,1.2V的电压输出无法稳定,以约1HZ的频率从1.1V抬升至1.4V,然后瞬间掉到1.1V,如此循环。而标称2.5V的电压实际输出约为2.62V。请问可能的原因在何处?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS75003
你好,我打算使用TI的TPS75003芯片为altera的EP3C10芯片供电。电路采用了芯片手册FIG2所示的典型电路。在空载情况下测试,1.2V的电压输出无法稳定,以约1HZ的频率从1.1V抬升至1.4V,然后瞬间掉到1.1V,如此循环。而标称2.5V的电压实际输出约为2.62V。请问可能的原因在何处?谢谢。
Hi
应该是输出电容的问题,您可以参考datasheet对于输出电容的要求:
The output capacitor is selected based on output voltage ripple and transient response requirements. As a result of the nature of the hysteretic control loop, a minimum ESR of a few tens of mΩ should be maintained for good operation unless a feed-forward resistor is used. Low ESR bulk tantalum or PosCap capacitors work best in most applications. A 1.0uF ceramic capacitor can be used in parallel with this capacitor to filter higher frequency spikes.