Other Parts Discussed in Thread: UCD3138, UCD3138HSFBEVM-029, UCD3138PSFBEVM-027
如题,用的是PMBUS烧写程序,JTAG和SCI口未使用
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: UCD3138, UCD3138HSFBEVM-029, UCD3138PSFBEVM-027
如题,用的是PMBUS烧写程序,JTAG和SCI口未使用
主函数main.c文件中是这样的
init_gpio();
init_pmbus();
init_dpwm();
init_adc12();
init_protection();
init_voltage_loop();
init_current_loop();
init_light_load_configuration();
init_miscellaneous();
init_timer_interrupt();没有这一类的函数调用文件,我想知道程序运行时芯片是怎么工作的?毕竟是从主函数开始运行,如果没有调用函数,程序是怎么执行的?
UCD3138的程序分成如下几大部分:
1. 背景环,即for循环(死循环),初始化完成后,程序一直在其中运行;
2. 标准中断,每100us或200us产生一次标准中断(时钟中断),用以运行状态;
3 快中断,有异常故障等场景时,触发快中断。
因此,程序的执行是这样的:程序一直运行在背景环,等待标准中断或快中断的触发。
时钟中断是这个函数:init_timer_interrupt();
通过这两个语句知,函数还使用了DPWM2周期中断和模拟比较器中断
write_firqpr (0x0A000000); //make them all irqs except FAULT_INT, DPWM2
write_reqmask(0x0A020000); //enable FAULT_INT and PWM0_INT, DPWM2
而DPWM2周期中断和模拟比较器中断的初始化是通过下语句完成的:
FaultMuxRegs.ACOMPCTRL0.bit.ACOMP_B_INT_EN = 1; //enable ACOMP-B interrupt
FaultMuxRegs.ACOMPCTRL2.bit.ACOMP_E_INT_EN = 1; //enable ACOMP-E interrupt
Dpwm2Regs.DPWMINT.bit.PRD_INT_EN =1;
明白了,这个程序应该是在调试时使用的,屏蔽了各个中断。
现在只是配置DPWM2 和 DPWM3发固定占空比的脉冲出来。因为调用了pmbus_handler(); 是可以下载和通信的。
正常的程序是不能这样设计的。
可以请那位TI工程师确认下,这个程序应该只是开环调试使用的,不是最终版本的。
我手上有这份程序(不一定是最新的),其中main.c的内容如下,请参考:
#define MAIN 1
#include "system_defines.h"
#include "Cyclone_Device.h"
#include "pmbus_commands.h"
#include "pmbus.h"
#include "variables.h"
#include "function_definitions.h"
#include "software_interrupts.h"
#include "cyclone_defines.h"
void init_interrupts(void)
{
TimerRegs.T16PWM2CMP0DAT.all = 1587; //Threshold to send the pwm low. Approx 10KHz. by spec.64ns clock period
TimerRegs.T16PWM2CMP1DAT.all = 0xffff; //Threshold to send the pwm high
TimerRegs.T16PWM2CMPCTRL.all = 2; //Enables compare 0 (reset) interrupt
TimerRegs.T16PWM2CNTCTRL.all = 0x00c; //PWM counter is running & enables PWM counter reset by compare action on compare 0
// FaultMuxRegs.EXTFAULTCTRL.bit.FAULT1_POL = 1; //rising edge
// FaultMuxRegs.EXTFAULTCTRL.bit.FAULT1_INT_EN = 1; //enable fault detection pin interrupt
// FaultMuxRegs.EXTFAULTCTRL.bit.FAULT1_DET_EN = 1; //enable fault detection
// MiscAnalogRegs.IOMUX.bit.JTAG_DATA_MUX_SEL = 3; //TDO/TDI Pin Mux Select as: Fault0 & Fault1
disable_interrupt();
disable_fast_interrupt(); //make sure fast interrupt is disabled
write_reqmask(CIMINT_ALL_PWM2_COMP | CIMINT_ALL_FAULT_MUX);//CIMINT_ALL_DIGI_COMP);
write_firqpr (CIMINT_ALL_FAULT_MUX);
enable_fast_interrupt();
enable_interrupt();
}
/*
Dpwm0Regs.DPWMINT.bit.PRD_INT_SCALE = 1; // generate an interrupt on each 16 switching cycles(used to reset the integrator)
Dpwm0Regs.DPWMINT.bit.PRD_INT_EN = 0;
disable_interrupt();
disable_fast_interrupt(); //make sure fast interrupt is disabled
write_reqmask(CIMINT_ALL_DPWM0 | CIMINT_ALL_PWM2_COMP ); //enable pwm2cmp and DPWM0 interrupt(End of 16th period)(int-priority29)
write_firqpr (CIMINT_ALL_DPWM0); // DPWM0 interrupt(End of 16th period) is mapped to FIQ
enable_fast_interrupt();
enable_interrupt();
*/
void init_variables(void)
{
supply_state = STATE_IDLE;
//supply_state = 12;
current_share_kp = 1000;
current_share_ki = 10;
fault_status = 0;
debug_buffer[0]=1;
debug_buffer[1]=2;
debug_buffer[2]=3;
debug_buffer[3]=4;
debug_buffer[4]=5;
debug_buffer[5]=6;
debug_buffer[6]=7;
debug_buffer[7]=8;
}
void main()
{
volatile unsigned int dummy;
if(GioRegs.FAULTIN.bit.FLT3_IN == 0)// Re-Check pin assignment (ADC_EXT/SYNC may be?)
{
//clear_integrity_word();
}
init_gpio();
restore_default_all();
init_variables();
configure_vin_on_off_thresholds();
configure_vout_cmd();
configure_ton_rise();
init_vout_fault(); // Analog comparator B
init_uart0();
init_pmbus();
init_front_end0();
init_front_end1();
init_front_end2(); //
init_filter0();
init_filter1();
init_filter2();
look_for_interrupted_dflash_erase();
init_ipri_cycle_by_cycle();
// init_cpcc();
current_share_int_state = (EADC_DAC_TARGET << CS_INT_EXP);
#ifdef SINGLE_FRAME_ENABLE
init_dpwms_for_single_frame();
#else
init_dpwms();
#endif
init_loop_mux();
handle_light_load_mode_configuration();
// init_current_sensing_hardware();
init_ADC_polled();
init_faults();
#ifdef IDE_ENABLE
init_ide();
#endif
init_prebias();
init_interrupts();
dummy = FaultMuxRegs.FAULTMUXINTSTAT.all;
Dpwm3Regs.DPWMCTRL1.bit.GPIO_A_EN = 1;
Dpwm3Regs.DPWMCTRL1.bit.GPIO_A_VAL= 1;
FaultMuxRegs.DCOMPCTRL0.bit.CNT_THRESH = 1;
FaultMuxRegs.DCOMPCTRL0.bit.FE_SEL = 0;
FaultMuxRegs.DCOMPCTRL0.bit.COMP_POL = 1;
FaultMuxRegs.DCOMPCTRL0.bit.THRESH = 850;
FaultMuxRegs.DPWM0FLTABDET.bit.DCOMP0_EN=1;
FaultMuxRegs.DCOMPCTRL0.bit.INT_EN=1;
//FaultMuxRegs.DCOMPCTRL0.bit.CNT_CLR = 1; //clear DCOMP reading
//FaultMuxRegs.DCOMPCTRL0.bit.CNT_CLR = 0;
FaultMuxRegs.DCOMPCTRL0.bit.COMP_EN=1;
for(;;)
{
if (erase_segment_counter > 0)
{
erase_task();
}
pmbus_handler();
// FeCtrl0Regs.EADCDAC.bit.DAC_VALUE=800;
/*
if (Interrupt_Flag==3)
{
//Dpwm3Regs.DPWMCTRL1.bit.GPIO_A_VAL=1;
//disable_fast_interrupt();
//write_firqpr (0x00000000);
CimRegs.FIRQPR.all = (0x00000000);
} */
}
}
/*
if (Interrupt_Flag==3)
{
Dpwm3Regs.DPWMCTRL1.bit.GPIO_A_VAL=1;
disable_fast_interrupt();
}
*/
//Dpwm0Regs.DPWMINT.bit.PRD_INT_EN = 0;
//
// CimRegs.FIRQPR.all = (0x00000000);
#pragma INTERRUPT(c_int00,RESET)
void c_int00(void)
{
main();
}
这个是PSFB的主函数吗? 还有除了主函数文件,其他文件应该也有不同,能不能麻烦通过附件把整个程序给我,压缩成rar后应该可以发过来的,闭环的PSFB程序
TimerRegs.T16PWM2CMP0DAT.all = 1587; //Threshold to send the pwm low. Approx 10KHz. by spec.64ns clock period
TimerRegs.T16PWM2CMP1DAT.all = 0xffff; //Threshold to send the pwm high
TimerRegs.T16PWM2CMPCTRL.all = 2; //Enables compare 0 (reset) interrupt
TimerRegs.T16PWM2CNTCTRL.all = 0x00c; //PWM counter is running & enables PWM counter reset by compare action on compare 0
Dpwm2Regs.DPWMINT.bit.PRD_INT_SCALE = 2; // generate an interrupt on each 16 switching cycles(used to reset the integrator)
Dpwm2Regs.DPWMINT.bit.PRD_INT_EN = 1;
您好,请问您黄色的那句话表示的意思是什么?我参考了技术文档,但是没有太理解他的意思
This value scales the period interrupt signal from an interrupt every switching cycle to 16 switching cycles,是说将上面PWM2的compare中断变成每16个周期触发一次吗?也就是每过16次compare 匹配进一次中断吗?然后给它赋值为2又是什么意思呢?
意思就是调整中断时间为每个周期进一次中断,或者N个周期进一次中断的意思啊。
Bits 3-0: PRD_INT_SCALE – This value scales the period interrupt signal from an
interrupt every switching cycle to 16 switching cycles
0000 = Period Interrupt generated every switching cycle (Default)
0001 = Period Interrupt generated once every 2 switching cycles
0010 = Period Interrupt generated once every 4 switching cycles
0011 = Period Interrupt generated once every 6 switching cycles
0100 = Period Interrupt generated once every 8 switching cycles
0101 = Period Interrupt generated once every 16 switching cycles
0110 = Period Interrupt generated once every 32 switching cycles
0111 = Period Interrupt generated once every 48 switching cycles
1000 = Period Interrupt generated once every 64 switching cycles
1001 = Period Interrupt generated once every 80 switching cycles
1010 = Period Interrupt generated once every 96 switching cycles
1011 = Period Interrupt generated once every 128 switching cycles
1100 = Period Interrupt generated once every 160 switching cycles
1101 = Period Interrupt generated once every 192 switching cycles
1110 = Period Interrupt generated once every 224 switching cycles
1111 = Period Interrupt generated once every 256 switching cycles
Jason 你好。感谢你的回答。还有一个问题想请教你,我在029EVM的configuration_function.c里面看到了一段代码:
void configure_vout_cmd(void)
{
struct qnote constant_DAC_VALUE_SCALER = {DAC_VALUE_SCALER, 0};
pmbus_dcdc_config_translated[0].vout_cmd = qnote_linear16_multiply_fit14(constant_DAC_VALUE_SCALER, pmbus_dcdc_config[0].vout_cmd, -VOUT_MODE_EXP);
FeCtrl0Regs.RAMPDACEND.all = pmbus_dcdc_config_translated[0].vout_cmd;
}
其中,DAC_VALUE_SCALER=996,是宏定义的,请问这个乘法函数表示什么意思呢?为什么是设置为996? pmbus_dcdc_config[0].vout_cmd=6144,VOUT_MODE_EXP=9,这样算下来刚好是11952,赋值给DCA作为电压环的12V。 我不明白的是996的来历,以及VOUT_MODE_EXP=9的含义,希望您能给我解答一下,不甚感激!
而且{DAC_VALUE_SCALER的说明是:DAC_VALUE_SCALER is included to convert the voltage to DAC LSBs. 但是根据TI的相关资料显示,DAC单位是1.5625mv/bit.
能把你的UCD3138HSFBEVM-029的原代码发我一份吗,我买了这款DEMO板,至今没有申请到程序,zszwnm@126.com 或者加我QQ348440333.我们聊聊一些合作的事情