This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,首先这个系统指的是SYS的输出,然后我们观察当电池进入深度过放时电池的端口电压低于3.0V,当适配器插入以后,如果Q4完全打开,那么相当于SYS与Battery的正极短路,那么此时SYS的电压就等于进入过放的电池端口电压,即低于3V,如果SYS接的是一个MCU ,其最低工作电压门限是3.3V(具体门限大小在REG01[3:1]设置),那么此时由于SYS被电池拉低到低于3V,此时MCU是不能正常的开机的,这样就导致必须要等到电池电压升高到3.3V以上才能正常的工作。这就是说明书中说的此时系统不能工作的意思,即SYS被电池端口电压拉低到低于3.3V。谢谢!
关于Q4,它在此时的作用就是实现了Narrow VDC Architecture,因为Q4完全打开以后,电池端口电压与SYS电压完全一致,所以我们需要Q4工作在LDO状态,即此时Q4作为一个调整管,等效于一个恒流源,通过不同的g-s电压允许不同的充电电流通过,这样由于Q4分担了一部分电压,所以此时SYS的电压就等效于buck电路的输出设定电压4.2V大于MCU系统设定的最低门限3.3V,此时MCU系统能正常的开机,而不用等到电池端口电压上升到3.3V以上。谢谢!
1)对于说明书的解读,二楼已经解释清楚。
2)对于Q4的作用,直观地理解是控制电池与系统的连通程度。可以实现:
a. 电池没多少电时,使电池与系统不完全连通,不至于把系统电压拖低而关机;
b. 运输或长期不用时,使电池与系统完全隔离,让电池电量储存更久;
c. 需要电池向系统供电时,使电池与系统完全连通;
d. ……