This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps75003电压问题

Other Parts Discussed in Thread: TPS75003, LM26420

现在用TPS75003给FPGA——EP3C5E144I7供电,tps75003电路与其官方技术文档上的电路一样,出来3路电压分别为1.3V,2.5V,3.3V(理论上为1.2V,2.5V,3.3V),但是将FPGA焊接上后,其中2.5V的电压就跌落到1.2V左右,重新换FPGA和电源芯片,效果一样。

               如果割开进入FPGA的2.5V电源电压,2.5V恢复就正常。

                如果割开进入FPGA的1.2V和3.3V电源电压,2.5V电压也恢复正常。

                如果割开进入FPGA的1.2V和3.3V其中的一路电压,2.5V电压变为1.8V左右。

请问这是为什么?仔细检查了原理图并没有发现不对的对方,参数也和官方文档一样。测量各个管脚与地也没有短路现象

        tps75003的3路电压应该是互不干扰才对,为什么3路电压会有影响?

        tps75003的2.5V电压如果出现跌落,会和那些有关?

        怎么样判断tps75003是否损坏?

  • 简单的检测TPS75003是否损坏,可以用相应的电子负载分别接三个输出来看是否正常。

    TPS75003的2.5V输出是个300mA的LDO,可能性最大的原因是过载。

    芯片的三路电源理应是互不干扰的。建议先用电子负载排除芯片损坏的可能,如果芯片正常,按照你之前的测试,有如下怀疑:

    割开进入FPGA的2.5V,LDO空载,输出正常;(割开状态下带个300mA的负载看看)

    割开进入FPGA的1.2V和3.3V电源电压,FPGA不工作,2.5V空载输出正常;(此时在1.2V和3.3V上带载来验证)

    割开进入FPGA的1.2V和3.3V其中的一路电压,FPGA工作不正常,2.5V轻度过载;

    三路全连,FPGA满负荷工作,2.5V这路过载。

  • 请问你的问题解决了吗?我也刚想要用TPS75003的官方PDF上的原理图给EP3C供电的  听你这样一说有点不敢用了 有没有找到原因?

  • 有条件的话就用电子负载模拟3路供电或者直接用电流钩表测试2.5V的实际带载状况。

    但是理论上三路并无关联,2.5V的负载应该是受到FPGA  1.2V和3.3V的影响而超出300mA.

  • 如果确认都是LDO带载能力不够,可以额外增加一个LDO, 如500mA的TPS73525等,Buck 部分则可以改为两路供电的 LM26420等。