This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EV2300的使用



我有几个关于EV2300的使用的问题,特请教TI技术人员,请赐教.

1)    在DATARAM显示屏上按下START  LOGGING 按钮后,CONTROL栏数据VALUE出现FA1A;FA1B;FA1C等字符串.这表明什么意思?

2)    在学习过程中,使用EV2300时,如何发布0021跟踪命令和0041复位命令呢?

3)     BQ系列电量计量表的精度是如何计算的?

谢谢!

  • 1.你使用的是那颗电量IC?

    2.就是在control栏输入命令,再开始学习。

    3.建议你根据gas gauge报告的使用时间来和实际的做比较。

  • 1.具体使用的是哪款电量计芯片?打开软件时确保软件与电量计固件版本匹配,没有提示任何不兼容的信息。

    2.在learning过程中,不要发送0021和0041命令,正常的learning过程是先不使能QEN,即QEN保持绿色旗标,将电池放空后等待5个小时后再DATARAM里control/manufacture中发送0021使能QEN,然后充电至100%即FC置1,等待2个小时后放空,再等待5个小时,这是有效的learning过程,中间过程不要随意发送0021和0041。

    3.电量计的精度可以通过一定的温度条件下,设定恒定放电电流,在电流经过校准保证精度的条件下,放电并记录全部放电数据,根据打印数据手动计算电流积分数据,即电流栏和时间栏的积分,加总后得到总电量,每一段的积分值再除以总电量就可以得到实际的电量百分比,和电量计上报的电量百分比作对比即可。