Other Parts Discussed in Thread: LM2576
用参考电路设计了一个20V输入15V输出的电路,不带负载时纹波很小,带一个100欧姆的电阻,纹波就有400mv多了
电路如下
示波器交流纹波如下
电感不合适?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM2576
用参考电路设计了一个20V输入15V输出的电路,不带负载时纹波很小,带一个100欧姆的电阻,纹波就有400mv多了
电路如下
示波器交流纹波如下
电感不合适?
楼主, LM2576的工作频率是52kHz,但是图片中的纹波频率显示为100Hz左右的低频纹波,所以建议楼主测试一下带载100欧姆情况下输入电压的情形,以及SW引脚的波形。另外请再确认一下电感的感值。
Hi
输出电容可以采用并联的方式获得较低ESR, 这个与纹波有关,但是ESR也不能太低,需要大于30mohm, 建议您找一些低ESR的电容作为输出电容(可以采用搭配,或者并联)