Other Parts Discussed in Thread: UCD9222, UCD7242
原理图参考的EVM板。整板用12V供电,并且在12V输入端做了一个电源监控电路。
现在DSP核电压一上电,12V就会关电保护。将VCC1V0端的电感去掉后,上电就不会保护了。
抓了一下VCC1V0和CVDD端电感的波形,对比了一下,发现VCC1V0的占空比很大,而且频率也不对,抓的这个波形频率看上去对,但是大部分时间里这个PWM的频率不稳定,一直在抖动。CVDD的波形是对的,输出电压也对。波形见附件。1通道:VCC1V0的PWM,2通道:CVDD的PWM
UCD9222的配置文件从研华官网下的,并且其他板卡是ok的,只有一块板卡有这样的问题。
后来将UCD9222和UCD7242都更换了一下。在更换之前,只是偶尔会保护,不过DSP的两路1V始终都没有输出。更换两个器件后,每次都会保护。
请TI工程师帮忙分析一下,谢谢