This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5521: 芯片的应用问题

Part Number: LP5521


CLK_32K脚位这个管脚不接时钟,接地会对功能上有影响么?例如呼吸灯效果等

  • HI

       If external clock is not used on the application, connect the CLK_32K pin to GND to prevent floating of this pin and extra current consumption.

       如果你不用外部CLK, 就会选用内部CLK, 对功能上没有影响,  差别只在于你的选择。对于选择外部CLK的优势,见datasheet 第17页 7.3.5.5