This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982: 与TPS65981的配合

Part Number: TPS65982
Other Parts Discussed in Thread: TPS65981

你好,

我们有一款产品分两个部分,都由电池供电,当一方的电池没电时可以互相通过USB-TYPEC供电,TYPE-C VBUS输出会从5V切换到12V。我们在两部分里面用的都是贵司的TPS65981,现在这个芯片几乎买不到了,我们就新设计了一个用TPS65982(虽然这个芯片也是不推荐新设计使用,但好像市场上还可以买到一些)。现在的问题是

我把原来的TPS65981的固件直接写进TPS682的flash里,发现只有当两部分都使用TPS65982时5V才会切换到12V,当一边用TPS65982,一边用TPS65981时,TPS65982做为source方只输出5V,但不会切换成12V,请问一般这是由于什么原因?可以解决吗?还是只能时65982配合65982?

5V输出用的是internal 5V power path, 12V输出用的是Internal high voltage power path; PP_EXT用作input