This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25710: BQ25710输入限流

Part Number: BQ25710


调试BQ25710只能带动48W的负载。输入电流达到5.5A就被限制了,软件中IDPM设置为6400mA。BQ25710EVM-017评估板也是一样的情况,采样电阻用的是10毫欧,,请问怎么提高输入电流能力

  • 您好,正在询问更了解这款芯片的TI工程师,稍后回复。

  • 您好,附件是BQ25710的寄存器配置日志,请查收。对于限流有如下疑问:

    * Created: Fri Feb 24 09:40:09 CST 2023
    *
    * Format: Register Name  tab Character,\t  Hexadecimal register value.
    * Device: bq25710
    * BQZ Container: Charger_1_00-bq25710.bqz
    *
    Charge Option 0	071F
    Charge Current Register	0BC0
    Charge Voltage Register	3328
    OTG Voltage Register	0000
    OTG Current Register	0000
    Input Voltage Register	0580
    Minimum System Voltage	2400
    Input Current Register	7F00
    Charge Status Register	8000
    Prochot Status Register	A800
    Input Current Limit In Use	7F00
    VBUS and PSYS Voltage Read Back	9100
    Charge and Discharge Current Read Back	0000
    Input Current and CMPIN Voltage Read Back	0000
    System and Battery Voltage Read Back	6301
    Manufacture ID Read Back	0040
    Device ID Read Back	0089
    Charge Option 1	0250
    Charge Option 2	021D
    Charge Option 3	0000
    Prochot Option 0	4A65
    Prochot Option 1	81A0
    ADC Option	A05F
    LOUT	0004

    1. 调试发现寄存器ChargeOption3的Bit[4:3](IL_AVG)的设置对输入限流有影响。我之前调试是设置为0-6A,目前将IL_AVG调整为15A后输入限流正常了。请问IL_AVG的设置是否真的会影响器件的限流?

    2. 如果我想要更大的输入电流,那么软件中RSNS_RAC设置为10 mΩ ,而硬件的实际采用电阻用5 mΩ ,这种方法是否可行?

    3. IDPM这个功能是如何体现的?因为在调试过程中(不接电池)发现使能和禁用寄存器 ChargeOption0 的Bit1(EN_IDPM)对限流没有影响。

  • 补充: 目前调试输入电压是12V和19V,但是我们的主板设计是要满足9-22V适配器供电,且主板满功率运作时功率会有100W。电池是3串,最小系统电压设置为9V,但是目前的调试阶段还不接电池。

  • 您好 

    1,2,正在询问更了解这款芯片的TI工程师, 晚点回复。

    3,CELL_BATPRESZ没有接电池是低,When CELL_BATPRESZ pin is LOW, the charger automatically disables the IDPM function by setting EN_IDPM (REG0x12[1]) to 0. T

  • 您好

    在论坛看到了TI工程师的回复,目前已经解决问题,非常感谢您们的支持!

  • 您好,很高兴您的问题已经解决。