This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61196-Q1: 使用TPS61196-Q1时,首先要在PWM端输入恒流电才能工作的问题

Part Number: TPS61196-Q1

Hi, all engineers,我现在使用TPS61196-Q1方式如下:

VIN = 12V。PWM最大为1KHz。但在按此原理图的使用过程中发现如下问题:

1.PWM端首先要输入5V恒流电(0.01~5s),再切换为PWM信号芯片才可正常工作。

2.在1的使用条件下,上电初期时我想拉低EN以此来防止5V恒流所导致的OUTPUT过大的问题。但是发现在PWM端输入5V恒流电时,EN无法禁止芯片升压。(LED工作电压36V)

如有类似问题或见解,望解答。

感谢。