Hi ti team,
请帮忙看下是否有匹配的型号推荐,谢谢!
Input: 85 VAC – 265 VAC Input
Output: 有效功率1500 W ( 50VDC@30A)
主动式PFC大功率开关电源 LLC ,输出有效功率1500 W ( 50VDC@30A) (恒压 ,过载,高温,短路,过压 保护)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
PFC可以选择UCC28070A之类。
第二级电源还可以选择全桥移相UCC28950.