This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ77910编程后工作状态的问题



各位大侠你们好:

   我使用EVM 板做实验,我们使用6节锂电池,并且都使用电阻来模拟电池观察BQ77910工作状态。

   芯片各寄存器数据如下:

1 is 80

2 is 38    

3 is 62  

4 is c

5 is c1

6 is 4    

7 is f

8 is 0

9 is f0

A is 33

上电后有如下现象:

1.PACK+和 BAT- 接电源(稳压电源24V),DSG CHG 没有12V输出。

2.将CHGST拉高后,DSG CHG 都有12V输出。但是大概7秒钟 DSG CHG无电压,LDO输出为零,芯片休眠状态。

求解:正常情况下,BQ77910是如何工作的?