TPS5430现在是否有PIN对PIN可替代的其它电源芯片?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
暂时没有找到与TPS5430的P2P的芯片。但可以使用比较接近的芯片TPS54233,开关频率为300K,但其输入电压
最高为28V.
附件是SWIFT系列芯片的参数对照表,供参考。
建议增加磁珠可以有效降低EMI(之前有不少客户通过加磁珠解决了EMI问题), 例如附件中磁珠规格或者其他的都是可以,如1000ohm/100MHz 的磁珠, 高频阻抗尽量大一些,效果会比较好。
snubber就是在PH脚到地接一个电容和电阻的串联,你可以先尝试把RC时间常数设在50MHz,电阻1欧左右。有效果的话再做调整。
另外也可以在BOOT电容上试着加个几欧的电阻看看。
LM22676 pin to pin compatible with TPS5430