Part Number: LM4140
使用LM4140-1.024时候(图上改为了1.024),按照图上GS8551放大,发现LM4140出来的基准电压会编程1.9V左右,我加大电阻R49,R50等改成10K跟随,还是会变。然后把电阻的阻值改成39K,则出来的基准电压为1.025V,然而不接电阻的时候出来的电压时1.024V还是会偏置0.001V,NSI1300D05出来的电压OUTP,OUTN为1.446V左右
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
将R50拿掉,直接测试基准输出是否是1.024V 来判定是否是LM4140芯片的问题即可。
如果是受运放这边或者其他芯片的影响,在确认电路设计。