This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61220: 无法使用powerdesigner输出0.2A的设计

Part Number: TLV61220


如下图所示,提示不符合设计,请问这个芯片最大输出电流是多少呢?我要接两节7号干电池做输入

  • Hi

        最大输出电流和最小输出电压有关,你可以查看datasheet第六页图1~3,  结合最小输入电压,和最小开关电流(红色)来查看最大可输出电流(纵坐标)。

        或者可以通过公式Vin*Isw/1.15 *效率= Vout* Voutmax   效率82%左右,Isw=180mA来评估最大输出电流。