你好,请问一下
IC spec有三种应用
1、Full Feature Application for Display Backlight
2、Application With Basic/Minimal Operation
3、SEPIC Mode Application 请问这三种运用时,频率以及电感感值是如何确定选择的,之前有个项目输出电流460mA/26.1V 选择 1818K、电感选择10UH 效率很低,更改频率400K效率OK。想要了解一下,频率以及电感是如何确认的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,请问一下
IC spec有三种应用
1、Full Feature Application for Display Backlight
2、Application With Basic/Minimal Operation
3、SEPIC Mode Application 请问这三种运用时,频率以及电感感值是如何确定选择的,之前有个项目输出电流460mA/26.1V 选择 1818K、电感选择10UH 效率很低,更改频率400K效率OK。想要了解一下,频率以及电感是如何确认的
Hi
你需要确认这三种情况下,输入,输出电压,总电流,然后按照这些参数来计算电感(Boost, SEPIC, 可以参照一般芯片的计算方式即可,参照附件3644.升压原理.pdf)
工作频率不宜选择太高,一般选择300~500kHz.
Hi
工作频率太低会造成功率电感感量过大,除了会造成电感尺寸较大。而频率太高一般会造成开关损坏过大。所以一般平衡下来300~500kHz较为合适。
boost是升压,SPICE是升降压,两个架构差异很大,功能前者是升压,后者可升可降,并且电路也负载一些。
HI
MOS选择在电压电流足够的情况下,Qg和Rdson尽量小就可以了。