This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z100芯片设计问题

Other Parts Discussed in Thread: BQ34Z100EVM

下列序号均指的是bq34z100EVM板上的元件序号,请教几个问题:

1、接两节以上磷酸铁锂电池的情况下,设置VOLSEL位为1,那是不是说明芯片VEN脚的输出恒定是为高电平?如果是的话,那设计电路的时候,是不是可以取消元件R2,R4,Q4和Q5?VEN引脚的描述上提到减小分压网络的功耗,如何减小?

2、BAT采集的是电池的电压,那2-3cell的磷酸铁锂电池的分压网络如何设置?芯片如何可以设置分压的比例大小?

3、在4灯显示模式的情况下,Q1,Q2的作用是什么?

4、在其他帖子看到说Q3是作用是降压限流,没有完全导通,相当于大电阻,G端稳定为5.6V,REGIN的输入电压稳到4V左右,那这个Q3的阻值会随电池电压变化吗?将Q3改为一个相应阻值的电阻可以吗?

  • 1、接两节以上磷酸铁锂电池的情况下,设置VOLSEL位为1,那是不是说明芯片VEN脚的输出恒定是为高电平?如果是的话,那设计电路的时候,是不是可以取消元件R2,R4,Q4和Q5?VEN引脚的描述上提到减小分压网络的功耗,如何减小?

    R:Ven不是恒为高,是需要采集COV条件时为高,不采集电池端口电压时就关闭了分压电路,从而节约了功耗。

  •  2、BAT采集的是电池的电压,那2-3cell的磷酸铁锂电池的分压网络如何设置?芯片如何可以设置分压的比例大小?

    R:If the battery contains more than one series cells, a voltage divider network will be required. Design the divider network, based on the formula below. The voltage division required is from the highest expected battery voltage, down to approximately 900 mV. For example, using a lower leg resistor of 16.5 KΩ where the highest expected voltage is 32000 mV:
    Rseries = 16.5 KΩ ( 32000 mV – 900 mV) / 900 mV = 570.2 KΩ
    Based on price and availability, a 600 K resistor or pair of 300 K resistors could be used in the top leg along with a 16.5-K resistor in the bottom leg.
    Set the Voltage Divider in the Data Flash Calibration section of the Evaluation Software to 32000 mV. Use the Evaluation Software to calibrate to the applied nominal voltage, e.g.: 24000 mV. After calibration, a slightly different value will appear in the Voltage Divider parameter, which can be used as a default value for the project.

  •  3、在4灯显示模式的情况下,Q1,Q2的作用是什么?

    R:p1 P2通过控这两个mosfet实现对两个led的亮灭。

  •  4、在其他帖子看到说Q3是作用是降压限流,没有完全导通,相当于大电阻,G端稳定为5.6V,REGIN的输入电压稳到4V左右,那这个Q3的阻值会随电池电压变化吗?将Q3改为一个相应阻值的电阻可以吗?]

    R:不能改成电阻,它是没有完全导通,但不能完全理解为一个电阻,这个管子此时分担一部分多余输入电压的作用,实际的输出电压大小与这个管子本身的特性有关,在这里它能起到钳制输出端电压大幅波动的作用,输出电压只会在4V左右波动,使用电阻没有这个效果。

    以上谢谢!

  • 1、SW开关这个是不是闭合的时候LED灯才会显示?没闭合的时候,灯都是灭的?如果利用74HC164扩展8个灯,是不是每个灯代表12.5%的电量?

    2、四灯模式下,为什么P3P4口不需要2SK3019?和P1P2口点亮的方式是相反的吗?

  • 能帮忙回答下吗,因为手中没有bq34z100EVM板