This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: 更换电池SOC显示0%

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQ34Z100

你好,
我的bq34z100应用在系统端(电池包外),现在已经获得CHEM ID,并且学习完成导出Gold image,但是将电池插上后SOC显示0%,RESET之后SOC显示100%,并且需要放电很长时间SOC才会下降,SOC开始下降之后还是比较准确的,更换电池之后SOC还是0%但是电压电流显示是准确的。
问题:
1.bq34z100应用在系统端需要注意什么
2.电池插入之后SOC显示0%怎么解决
3.更换电池SOC显示0%怎么解决
4.Gold image烧录之后都需要什么操作(例如RESET、IT_ENABLE)