Other Parts Discussed in Thread: UCC27524, UCC27201, UC2843, LM5022
我发现现在TI的Boost(外部开关)的芯片,对MOS管的驱动电压都是7~9V左右的,为什么没有驱动电压是12~15V的芯片呢?对于MOS管,驱动电压7~9并不是一个理想的电压。请问现在TI有输入范围较宽,驱动电压输出是12~15V的芯片吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想找一款像LM5022这样的能够直接承受输入电压的Boost芯片,耐压最好能到120V,驱动输出电压能到12V的芯片,随便问一下,LM5022的VIN的引脚是高阻态引脚吗?是否能用电阻分压进行输入?
您好,
个人觉得VIN是否能采用电阻分压进行输入主要取决于功耗。负载不同,分压电阻中间的VIN也会不同,分压电阻流过的电流也会不同,需要考虑分压电阻是否能承受如此大的功耗。 一般信号回路采用分压电阻的形式比较多,功率电路不太多。
对于由内部产生Vcc的这类芯片,个人了解的还没有做到120V以上的
lei zhang5 说:我想找一款像LM5022这样的能够直接承受输入电压的Boost芯片,耐压最好能到120V,驱动输出电压能到12V的芯片,随便问一下,LM5022的VIN的引脚是高阻态引脚吗?是否能用电阻分压进行输入?