This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ20Z65R1短路测试

Dear All:

         本人在测试一部电池使用的IC型号为BQ20Z65R1,在测试短路时发现AFE SC DSG CFG 只有设置成0F(27.5A  0uS)时,SCD 标志位才点亮。如果设置成1F(27.5A 61uS),SCD标志不点亮。电路原理图较成熟,不存在原理图错误的情况,PCB布线按照TI官方的布线规则。

        个人假设如下原因:(1)ASRP,ASRN两条线, PCB布线时阻抗太小------测试之后排除。(2)短路电流超过超过IC检测范围,但AFE SC DSG CFG 只有设置成0F(27.5A  0uS)时,SCD 标志位点亮,示波器显示电流(27.4A 62.3uS)就可以保护----排除。(3)布线不正确?经大家确认布线正确的-----排除。(4)与整体的阻抗有关包括{电池,MOS,敏感电阻,PCB}----有待确认。

      目前暂未得到解决办法,望专家帮忙分析原因(能有决绝办法的请回复)。

Thanks,

       

  •         本人通过测试直接短路得出结果为(91.5A,750us)说明已经超出IC检测范围,故SCD不会点亮,如果使用负载27.5A,SCD点亮。但如何解决直接短路SCD不点亮的问题是我现在需要思考的,请大家给我点意见。如何把ASRP,ASRN两条线钳位在正常范围。