This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65251 一接负载板就烧掉了

Other Parts Discussed in Thread: TPS65251

你好,我的产品分为两块板子,TPS65251板和负载板,TPS65251输出1V/2A,3.3V/3A,5V/2A,不接负载板时,tps65251输出正常,接上负载板后,TPS65251电压不稳定,过一会后,TPS65251电源无输出,测量知:TPS65251 的V3V对地短路,请问下这个是什么原因。电路是按照demo板设计的

  • 首先需要说明的是只有buck具备3A的输出能力,因此第一路要做成3.3V输出。调试加载的时候建议采用慢慢调的形式,不确定不要突然加全载。

    3.3V的bypass电容没有漏吧,layout上要靠近芯片。芯片layout要参考DEMO板,底部的powerpad要充分的焊接和扩展用作散热(并且是接GND的),注意datasheet 第二十四页layout说明。

    是否还有其他的脚阻抗上异常,例如Vin1/2/3或者LX1/2/3?  

  • 你这个问题我有遇到过,跟Layout 的关系很到,请问是几层板。

    TPS65251 至少要 4层板,而且 TOP 层的 地要完整,如果留的空间太小,很容易烧

  • 按常理分析是加载时开关出力产生反电动势高于芯片的规定电压,在IC到电感之间加一个TVS管和电阻,这两个原件串起来,或加快复二极管