Other Parts Discussed in Thread: GPCCEDV
满电后,恒流放电时,RSOC电量百分比突然掉下去,如log中提示,从80%突然掉到7%了,什么原因?
所有的参数都经过CEDV学习后的参数,并CEDE-report参数,经ti的工作人员确认是ok的:e2echina.ti.com/.../bq4050。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
GPC_CEDE:
GPC CEDV tool, rev=60
Configuration used in present fit
ProcessingType=1
NumCellSeries=1
CellTermV=2500
LearnSOC%=7
FitMaxSOC%=9
FitMinSOC%=3
ChemType=4
ElapsedTimeColumn=0
VoltageColumn=1
TemperatureColumn=2
CurrentColumn=3
CEDV parameters resulting from the fit. If EDVV bit is set to 1, EMF and EDVR0 have to be multiplied by the number of serial cells when written to data flash
EMF 3558
EDVC0 427
EDVC1 0
EDVR1 231
EDVR0 1446
EDVT0 1106
EDVTC 11
VOC75 3317
VOC50 3291
VOC25 3240
Recommended SOC deviation tolerance at EDV2 point is < 5% for low temperature and <3% for room and high temperature
Deviations for this set of parameters are given below for each file
file SOC error, % pass
roomtemp_lowrate.csv 1.03935862717195 1
roomtemp_highrate.csv -1.00978888520085 1
hightemp_lowrate.csv -0.606935153142983 1
hightemp_highrate.csv -1.38639747773708 1
lowtemp_lowrate.csv -0.275100967537564 1
lowtemp_highrate.csv -0.840727922727811 1
Deviations are within recomended range. CEDV parameters are suitable for programming the gauge
************************************************
OCV11:
SOC, % OCV, mV
0 2513
10 3036
20 3097
30 3118
40 3145
50 3162
60 3177
70 3187
80 3191
90 3194
100 3301
我看到TMR文档有介绍,但看不明白这些公式。上面是CEDV-report的信息,请问应该如何来确定EDV0-EDV2的数据?

您好,CEDV模式,EDV0这些参数是不能读取的, BQ4050 为例,设置参数 Settings >> Configuration >> CEDV Gauging Configuration [EDV_CMP]=1 即可用 Compensated EDV,动态计算 EDV2/EDV1/EDV0 电压。
详细请参考下面文档3.2 CEDV 电量计算法原理
您好,
Max error just counts up as a function of senseR size and amount of charge accumulated. it gets reset to 2% when you get a value FCC update. The use is just a way to show that you have not successfully learned FCC in a while and you could have potential coulomb counter error accumulated.
FCCX will toggle for every FCC update performed. with a Max Error of 8% FCC learning was not done for some amount of time. Meaning a "qualified" discharge never happened for a bit.