TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z746: BQ27Z746试产问题

Part Number: BQ27Z746

各位专家好!

  目前BQ27Z746在第一次试产时遇到几个棘手的问题,还请帮忙解惑,谢谢!

1、试产1K中,PCBA烧录测试均OK,组成电池包后有100组左右出现不通信,充电无反应,量到TS引脚上有电压变化,这种情况下如何判断问题,是芯片坏了还是进入了什么特定的状态,电池组是否还有得救;

2、当在Settings里面打开AUTO_SHIP_EN时,电池在设定时间内进行shutdown mode,充放电MOS关闭,SDM置位,但是无法充放电,也不能退出SDM模式;看操作手册写的进入此模式需要ENAB拉高,但是我的ENAB是拉GND的,理论上是无法进入此模式的;另外不管在哪个模式下,充电应该也是能激活的才对?

  • 您好

    1,不能通讯,建议您和好的板子对比一下,哪里有异常。TS电压不对,请确认是不是热命电阻坏了。

    2,ENBA:Active low digital input with weak internal pullup to VDD. If enabled for ultra-low power SHIP mode, driving this signal to the PACK– negative terminal will enable the device to wake up.