This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

寻可替换LM723的电源芯片



这是我现在用的电路,一个很老的电路了,用来驱动卤素灯。但是很稳定,纹波<0.1mV。就是TIP142发热巨大(电流1.7A),需要很大的散热片。

现在想要换一个效率更高,更稳定的电路,成本暂不考虑。要求如下:

输入12~15V,输出10~13V可调;

输出电流>=2A;

纹波电压<1mV;电流稳定度 <0.2%。

电路简单,功耗小。