TI老师好,关于LM2940使用,有些疑问再咨询一下:
1.Output Voltage Trimmed Before Assembly这个怎么理解?Mirror Image Insertion Protection这个怎么理解?这些在手册里哪些地方有说明呢?麻烦解答一下;
2.如下所示:
关于输出阻抗测试,是在100mADC and 20mArms f0=120Hz条件下测得,怎么要同时施加直流与交流信号,LDO输出阻抗到底怎么测试呢?请帮忙解答一下;
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI老师好,关于LM2940使用,有些疑问再咨询一下:
1.Output Voltage Trimmed Before Assembly这个怎么理解?Mirror Image Insertion Protection这个怎么理解?这些在手册里哪些地方有说明呢?麻烦解答一下;
2.如下所示:
关于输出阻抗测试,是在100mADC and 20mArms f0=120Hz条件下测得,怎么要同时施加直流与交流信号,LDO输出阻抗到底怎么测试呢?请帮忙解答一下;
谢谢!
Mirror Image Insertion Protection这个怎么理解?
Mirror-image insertion protection means that a regulator is designed for use when a voltage, usually not higher than the maximum input voltage of the regulator, is applied to its output pin while its input terminal is at a low voltage, volt-free or grounded. Some regulators can continuously withstand this situation; others might only manage it for a limited time such as 60 seconds, as usually specified in the datasheet. This situation can occur when a three terminal regulator is incorrectly mounted for example on a PCB, with the output terminal connected to the unregulated DC input and the input connected to the load. Mirror-image insertion protection is also important when a regulator circuit is used in battery charging circuits, when external power fails or is not turned on and the output terminal remains at battery voltage