不知道该怎么对BQ20Z45加电,要连接电池吗?还是直接对PACK口供电
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以参考user guide
http://www.ti.com/lit/pdf/sluu329
一般是在1N1P2P3P4P这几个端口接电芯,如果不满足4节,那么短接高节的端口,比如3节的话3P4P短接在一起。
2-4串电量计一般还需要激活,即短接4P和PACK+(实际终端客户可能采用插入适配器激活)。
连接EV2300,打开上位机软件即可看到通信。
如果不充放电的话,可以采用相同的电阻接到1N-4P端口分压,然后加一个电压在1N和4P之间。
我看了USER GUIDE 里面说的,要进行放电的话,要把SYS端PACK-,是的吗?。我的情况使这样的,我有了四个串联的电池18650,分别接到了1N1P2P3P4P这几个端口,另外通信端口接到EV2300,打开软件界面后无任何的信息啊,是我接错误了吗
PACK+和PACK-是接负载和charger的。首先确认一下电量计是否激活了。