This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LMZ12010的应用问题

Other Parts Discussed in Thread: LMZ12010

尊敬的TI工程师们,你们好 

我最近采用你们的LMZ12010做电源管理,我的输入是12V ,输出分别需要5V  ,我看到你们的datasheet上表格说明当需要输出5V时候,需要设置外部电阻分别是5.62K和1.07K,但是在后面你们提供的VO计算公式表明VOUT = 0.795V * (1 + RFBT / RFBB),带入计算发现输出电压时4.9706V,与5V有30mV的差距(此款芯片纹波显示为24MVPP),请问你们的表格数据是实际亲侧的嘛 ?

  • Hi

       芯片基准电压或者反馈电阻都是用精度公差的,所以5V输出也是有精度公差的。例如参考电压0.795的实际电压是0.775~0.815,公差是2.5%, 而分压电阻的精度通常是1%, 所以输出电压也是有一定精度的,就算在5V+/-3%也都是正常的.

  • Hi

       请问你是否对输出电压的精度是否有非常高的要求,基本上所有的DC/DC的芯片都与上述相似,输出电压是有一定公差范围的。

  • 楼主,除了电压都有一定的精度范围外,在实际设计中,电阻的阻值是一系列固定值,所以有时可能无法选择到合适的电阻使输出电压精确的等于设定值。

    此时,主要在精度范围内即可。或者采用多个电阻并联等方式,可以精确的得到设定值。