This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24170 充电电流问题

  按照数据手册设置好 

Ichrage=Viset/(20*Rsr)=1.5/(20*0.02)=3.75A;

Idpm=Vacset/(20*Rac)=1.6/(20*0.02)=4A;

但实际上对4000mhA 3.3V(当时电池电压)的锂电池充电时,只能测得1.7A左右的充电电流 。

问:是否设置有错误?还有其他因素影响?