This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28600

Other Parts Discussed in Thread: UCC28600

你好为什么UCC28600的VDD电压在5V到12V之间跳变

  • 您可以通过外部电源供应器直接供电15V到UCC28600 Vdd看变压器次级输出是否稳定,如果稳定则需要确认VDD的bypass电容10uF有没有。如果不稳定,则二次绕组出来的电压给到VDD也不会稳定,即会存在跳动,这个时候您就需要确认您的过电流设计,反馈设计以及变压器等有没有问题,这些都会造成VDD电压不稳定。

  •  你好!我在调试UCC28600D的时候给IC供18V电测试MOS管的驱动波形,发现没有波形,去掉MOS就有驱动波形,我是不是买到假货,请问下你电话号码多少,我想电话咨询下

  • Dongxu Mo 说:

     你好!我在调试UCC28600D的时候给IC供18V电测试MOS管的驱动波形,发现没有波形,去掉MOS就有驱动波形,我是不是买到假货,请问下你电话号码多少,我想电话咨询下

    Hi,

    一、建议首先用万用表检查一下MOSFET的漏-源和栅-源之间是否短路或者阻值很小。如果是的话说明MOSFET上电损坏,检查下电路中是否存在MOSFET过压或者直通的可能。

    二、检查下芯片的输出驱动能力是否足够。

  • 您好,

    可否提供下原理图看下。谢谢