This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LMZ31710的问题

Other Parts Discussed in Thread: LMZ31710

尊敬的TI工程师们,你们好

我在使用你们的这款芯片做电源管理,设计要求是3.3V(PVIN) 5V(VIN) ,输出1V ,输出电流5A,纹波要求20mv之内

我在查看他的DATASHEET 时,知道RSET应该是2.15K,但是这个阻值没有买到,所以我的问题是

1、可否使用2K(1%)和150欧(1%)的两个电阻串联来实现2.15K的设置电阻?

2、我使用你们的WEBENCH在线热仿真,发现在我的工作条件下,此款芯片的温度得达到70℃,请问这样的温度安全吗?

3、在PCB设计中请问有什么需要注意的来避免芯片过热