This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF5050



请问REF5050,我给12V的输入,它是5V输出,那么这个芯片发热量大吗??

  • HI

       不大,因为参考电压的电流需求一般非常小。

       即便按照最大10mA的电流,热阻150℃/W, 常温25℃下工作, 芯片的温度Tj=25+(12-5)*10m*150=35.5℃

       温升只是10.5℃,而实际应用中参考电流或可能少于1mA, 至更加的低,基本上不会造成什么发热。