This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

移動式電源充放電管理及保護



您好

計劃設計一單鋰聚合物電池,移動電源充放電管理,電池容量7500毫安

請教我要設計1C充電5v0.5c供電,要簡單,有輸出保護,電量簡易顯示

請提供該使用哪幾個晶片,感謝

  • 7500mAh还需要用1C充电,那么充电电流高达7.5A,这么大的电流目前chargerIC应该都支持不了吧,目前TI的bq2419x系列最高支持到4.5A已经是业界非常高的数值。如果要做7.5A的可能楼主需要采用DC-DC自行设计电路实现,另外可以考虑下采用多串的方案,这样子可以使用小点电流实现相同时间充进一样的能量。

    一般移动电源充电电流都没要求这么高,通常甚至还小于放电电流,所以请确认一下规格。

    电量计量的单串可以考虑bq27541,如果成本要求很高并且电流很大可以评估一下bq27621.