急需24V输入,5V输出的LDO,电流600mA-1A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
也可以选择性能高一点的TPS7A4700 http://www.ti.com.cn/product/cn/tps7a4700 之类。
按照你的条件,LDO的最大功耗高达9.5W, 建议前面增加一级DC/DC,提高效率降低功耗,否则只用LDO, 必须要非常好的散热设计,会比较麻烦。
楼主您好!
如楼上几位所述,这么大的压差和电流,单独用一个LDO损耗太大,热设计也不大好处理。所以建议用一级开关电源+LDO。开关电源的选择可以用TI的webench工具,如可以用LM25010. LDO 可以参考楼上的建议。
PS:LM25010选择参考:http://webench.ti.com/webench5/power/webench5.cgi?lang_chosen=zh_CN&VinMin=21.6&VinMax=26.4&O1V=5&O1I=1&op_TA=30
Hi Dali Ou
根据您是给5V ADC供电的
5V的LDO,我推荐楼主使用TPS7A4700系列 此LDO能够使得输出噪声仅有4uVRMS,同时具有很高的电源抑制比(PSRR)。
能够让您滤掉DCDC的输出纹波,给ADC提供纯净的电源。
Hisen Zhang
DCDC+ LDO是比较常见的选择:LM22672 LMZ13601 TPS5410 +TPS7A8101 TPS74801都是常见的选择