我这边有个客户提供的移动电源充放电保护板,用的是BQ24195的主芯片,还有TPS61090,430G2232还有两个TPS2511两颗控制两个USB输出,有人做过这个方案吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
bq24195自带同步升压DC-DC,不知道你客户提供的方案中用TPS61090的用处是什么。430MCU是用来控制bq24195的,TPS2511做充电识别和负载开关。这个方案应该说是比较常见的。
TPS61090 这个作用应该是做第二路输出的。如果只需要支持5V的输入并且一路的输出电流要求不大的情况下,可以考虑使用BQ24295,BQ24195比BQ24295的OTG电流大,但是如果加了DC-DC升压电路做大电流USB输出,那么BQ24295的OTG电流可能可以满足另一路需求。
如楼上所说这个方案是非常成熟的方案。