我目前遇到些问题:用的IC是与LM5017基本功能一致的LM34927.
1/规格书提到current limit:
"If the current in the buck switch exceeds 1.02A the present cycle is immediately terminated, and a non-resetable off-timer is initiated"请问这个current limit是在ON起作用,还是在OFF起作用,还是在ON OFF整个周期内起作用.我做了一个实验:当ON的电流1.02A的时候,就出现了current limit的现象,但是在OFF的时候就没有出现这种现象.
2/我设计的规格是:12V/0.08A的主反馈路输出,12V/0.08A,5V/0.1A,3.3V/0.1A的隔离输出.输入范围为17~75V,f=360KHz,L=33uH.
满载:主反馈路12V在18~24V输入的时候,输出电压变化比较快约为12.9~12.3的变化;在24~75V输入的时候,输出电压变化只有12.3V~12V.在18~75V时,工作是正常的.采用type2的方式增加纹波.
请问是什么原因导致18~24V输入的时候,输出电压变化比较快?如何得到比较良好的负载调整率呢?