Other Parts Discussed in Thread: TL494
根据TL494的DATASHEET可知,该芯片共有两个误差放大器(1,2,15,16脚),共用一个输出端(3脚),控制PWM的占空比,我的问题是:
1.当误差放大器开环使用时(第三脚未使用),放大器的输出电压是个多少V??
2.两个误差放大器的输出是连在一起的,若一个做为可调输出电压(将误差放大器连接的一段连接可调电位器,从而调整输出电压),一个作为输出电压的反馈输入用(稳定输出电压),两个放大器是同时工作吗??输出电压取决于那个放大器的输出??若两个误差放大器同时工作,工作原理是什么??
3.当输入电压时9-14V,输出电压时24V时,输出端连接到误差放大器的反馈电阻怎么选择,有计算公式吗??(比如,第15脚接固定参考电压5V,16脚接输出取样电阻,取样电阻的值怎么计算,也就是反馈到16脚的电压应该是多少??)
谢谢各位!