你好,请问使用BQ2057有个问题,电池电量已经接近充满,但是STATE管脚外接的LED灯依然不灭,需要把VCC充电电源略降,LED灯才熄灭,这是怎么回事?按道理说只要电池电压接近于满电压,STATE管脚就应该呈低电平,而和充电电压大小无关。请专家解答,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,请问使用BQ2057有个问题,电池电量已经接近充满,但是STATE管脚外接的LED灯依然不灭,需要把VCC充电电源略降,LED灯才熄灭,这是怎么回事?按道理说只要电池电压接近于满电压,STATE管脚就应该呈低电平,而和充电电压大小无关。请专家解答,谢谢
您好,我的电路设计中,VCC为9V,充电12 个小时以后,电源显示充电电流20~30mA,测得锂电池两端电压8V,STATE管脚电压3V左右,所接充电指示灯比刚充电时稍暗,但没有完全熄灭。
但继续充电,STATE灯依旧不会熄灭。如果充电完成的电流值是资料里说的14mA,那么实验过程中从没有达到这个阶段。如果想锂电池电压到达8V左右,就用充电指示灯指示电池已充满,请问应该如何改进?
还有,BQ2057如何感知充电电流?是通过VCC与VSNS之间的压差间接感知的吗?
方便的话能留一下邮箱地址,我把具体原理图发给您,请您指正一下。
是的,就是通过对SNS电阻上电压的采样来完成充电电流检测的。
充电电流还在截止电流(typical 14mA)之上的话,STAT是不会变化。
问题是为什么充了12个小时还有20多mA的电流,建议排查是不是锂电池的漏电流,亦或是后面还有什么负载?