调试过程输入电压和可调电源输出21V,电流4A,电池为12V铅酸电池
空载不接电池输出电压为13.8V
接上电池没有充电电流,此状态下各个电压如下:
VIN=21.027V
VCC=20.809V
Vmppset=1.4105V
Vref=3.299V
Vregn=5.964V
Vbtst=12.519V
Vph=12.519V
Vsrp=12.516V
Vspn=12.516V
VFB=1.9007v
还请大侠帮忙看看
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
调试过程输入电压和可调电源输出21V,电流4A,电池为12V铅酸电池
空载不接电池输出电压为13.8V
接上电池没有充电电流,此状态下各个电压如下:
VIN=21.027V
VCC=20.809V
Vmppset=1.4105V
Vref=3.299V
Vregn=5.964V
Vbtst=12.519V
Vph=12.519V
Vsrp=12.516V
Vspn=12.516V
VFB=1.9007v
还请大侠帮忙看看
您好,请参考下面内容:
1. The SRP and SRN line need to be connected directly across the sense resistor, routed differentially from the IC. It looks like SRN is connected after C98.
2. The TS network is incorrectly biased. Typically we recommend R152 and R153 when a thermistor is present in parallel with R153. Because there is no thermistor present, please bias TS between VHTF and VLTF. This is most likely your issue. I would recommend pulling up STAT1 and STAT2 through resistor and LED for future debugging.
3. For 4 A charge current we recommend 6.8 uH inductor and at least 20 uF output capacitance. I see 3.3 uH inductor.
4. We suggest a 20 uF input capacitance for 4 A charging current.